UL PUCCH Test Configuration
PUCCH Test Config Type
Couplings:
When PUCCH Test Config Type is ‘38.141-8.3.1 ACK missed detection for PUCCH format 0’, the ‘Number of symbols’ is visible to set.
When PUCCH Test Config Type is ‘38.141-8.3.4 UCI BLER performance for PUCCH format 3’, the ‘PUCCH Format3 Test’ is visible to select Test1 or Test2
When PUCCH Test Config Type is ‘38.141-8.3.4 UCI BLER performance for PUCCH format 3’ or ‘38.141-8.3.5 UCI BLER performance for PUCCH format 4’, the ‘Additional DMRS’ is visible to enable or disable additional DMRS. (For PUCCH Format 3 Test2, Additional DMRS is fixed to off).
Selects the PUCCH Test Config Type, the choices are defined in the section 8.3 of 38.141.
For ACK missed detection test, we use all ‘1’ as the payload.
For NACK to ACK detection test and UCI BLER test, we use PN9 as the payload.
Subcarrier Spacing
Selects the Subcarrier Spacing.
|
Subcarrier Spacing (kHz) |
FR# |
Channel Bandwidth (MHz) |
|---|---|---|
|
15 |
FR1 |
5 |
|
10 |
||
|
20 |
||
|
30 |
FR1 |
10 |
|
20 |
||
|
40 |
||
|
100 |
||
|
60 |
FR2 |
50 |
|
100 |
||
|
120 |
FR2 |
50 |
|
100 |
||
|
200 |
Bandwidth
Select the Bandwidth configuration for the carrier.
|
Subcarrier Spacing (kHz) |
FR# |
Channel Bandwidth (MHz) |
|---|---|---|
|
15 |
FR1 |
5 |
|
10 |
||
|
20 |
||
|
30 |
FR1 |
10 |
|
20 |
||
|
40 |
||
|
100 |
||
|
60 |
FR2 |
50 |
|
100 |
||
|
120 |
FR2 |
50 |
|
100 |
||
|
200 |
Duplex Type
Choices: TDD | FDD
Selects the duplex type.
When TDD is selected, several TDD parameters appear below. These TDD parameters are reset to default values whenever numerology changes or FR changes. (The default values are different for each numerology.)
Transmission Periodicity
Sets the periodicity of DL-UL pattern. The choices are related to numerology.
Number of Downlink Slots
Sets the number of consecutive full DL slots at the beginning of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Number of Downlink Symbols
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive DL symbols in the beginning of the slot following the last full DL slot.
Number of Uplink Slots
Sets the number of consecutive full UL slots at the end of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Number of Uplink Symbols
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive UL symbols in the end of the slot preceding the first full UL slot.
Number of Special Slots
Displays the number of special slots.
TDD Slot Allocation
Displays the TDD slot allocation for one period.
Phase Compensation
For waveform playback mode:
Choices: Auto | Auto (Real-time) | Manual | Manual (Real-time) | Off
For real-time uplink mode:
Choices: Auto | Manual | Off
Default: Auto
Sets the phase compensation mode on baseband signal before upconversion.
Auto | Auto (Real-time): Use the RF frequency from the instrument node.
Manual | Manual (Real-time): Enter the RF frequency manually.
Off: Disable phase compensation on baseband signal.
(Real-time) means the phase compensation is done using FPGA inside the instrument.
Number of Symbols
Choices: 1 | 2
Default: 1
Set the number of OFDM symbols when PUCCH Test Config Type is 38.141-8.3.1 ACK missed detection for PUCCH format 0.
PUCCH Format3 Test
Choices: Test1 | Test2
Default: Test1
Select the PUCCH Format3 Test when PUCCH Test Config Type is 38.141-8.3.4 UCI BLER performance for PUCCH format 3.
Additional DMRS
Choices: On | Off
Default: Off
Set additional DMRS for PUCCH format 3 and format 4.